1/9/2018 2:36 PM | |
Posts: 11 Rating: (0) |
Dear expert I have the PLC S7200 CPU 224xp I have Microwin V4.0 SP9 In that software I don't have any Analog blocks in library blocks S_RTR,S_RTI,S_RTI kindly suggest the procedure to add the tools in libraries. Rgards Arul ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 1/11/2018 1:04:31 PMNew subject after splitting |
|
1/9/2018 3:22 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Arul; These functions are part of the Scale library for MicroWin; you can download a zipped version of the library from the following FAQ, along with a link to a sample project ("TIP038", from the S7-200 Tips and Tricks): https://support.industry.siemens.com/cs/fr/en/view/27043396 Instruction to load a new library to MicroWin are also available in the Notes of the download. Hope this helps, |
Last edited by: Jen_Moderator at: 1/18/2018 3:13:52 PMInserted right link. |
|
This contribution was helpful to1 thankful Users |
Follow us on