10/12/2016 7:59 AM | |
Joined: 5/20/2015 Last visit: 4/24/2024 Posts: 216 Rating: (3) |
hello Experts I have s7-200 PLC and associated programming software Microwin. v4.0 sp9 I want to monitor Elapsed time on SCADA Runtime but when i configure T40 variable to output field it does not show Elapsed time. Whereas when I monitor Microwin it shows Elapsed value with timer like +123=T40, my query is how i will get variable for Elapsed time of the timer like T40 (100ms time base) Is there any special Syntax Like T40:ET...i have tried but it did not worked. thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/12/2016 10:40:21 AMNew subject after splitting Let's do it... |
|