1/28/2020 11:22 AM | |
Joined: 1/28/2020 Last visit: 1/16/2024 Posts: 7 Rating: (1) |
Hello I have a project in WinCC 2008 SP2 UP 13 (sinumeric option) (for windows XP) I need to migrate the project to WinCC 2008 SP5 (Windows 10). I migrate, but the Dctl object (communication between NC, WinCC PLC) does not work. All variables adrone directly to NC or PLC are wrong (no connection, variables are red) Of course unable to generate the project (.fwx) I suppose I miss some option on SINUMERIK ... I migrated directly from WinCC 2008 SP2 Up13 to WinCC 2008 SP5. Thank you for advice ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/28/2020 11:40:02New subject after splitting |
|
Follow us on