8/12/2014 11:31 PM | |
Posts: 10 Rating: (0) |
Hello Experts, I have a damaged Micromaster vector which iam migrating to MM420, the MM420 is connected through profibus to 316-2DP CPU. After commissioning and cofiguration I cannot run the drive from the PLC, it is giving F0070, I set my address P918=10 and the DIP swich on Profibus module is all OFF. Attached is the parameter settings through Drivemonitor, Kindly help check and revert. In r2050(0)=17534 and r2050(1)=8304 these values I receive from CB. Kindly advice on the parameterization. PLEASE AttachmentMICROMASTER_FinalBAG.zip (145 Downloads) |
8/13/2014 10:37 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello AutoGen_631805, What is the color of the Led on the MM4 Profibus Board? Try to increase P2040 (Pay Attention) Have a look: MICROMASTER 4 (MM4), SINAMICS G120 (CU240x DP): What are the possible causes of F0070 and how do I avoid them? Go to chapter 5: Operating Instructions: MICROMASTER PROFIBUS Optional Board MICROMASTER 4 (MM4): What is important when setting up an MM4 with a Profibus module? Read Umbi and Graeme: Upgrade from Profibus module 6SE3(9)290-0XX87-8PB0 to 6SE640X-1PB00-0AA0 for inverter chang |
Last edited by: Ste39 at: 8/13/2014 10:59 AMLast edited by: Ste39 at: 8/13/2014 10:54 AMLast edited by: Ste39 at: 8/13/2014 10:42 AMAdd FAQ Last edited by: Ste39 at: 8/13/2014 10:40 AM |
|
8/16/2014 11:45 AM | |
Posts: 10 Rating: (0) |
Many thanks Ste39 and Devesh. I have change the configuration in hardware with replacement with MM420 on profibus DP with my address 10 also Profibus status Green showing comms is OK. I checked my buffer in PLC diagnoses with the attached file, pls help analyse. Additionally give me hints on logic changes to make in software AttachmentDiagnose_CPU316-2DP.pdf (143 Downloads) |
Follow us on