10/8/2019 7:46 PM | |
Joined: 5/24/2019 Last visit: 10/27/2021 Posts: 12 Rating: (0) |
In "wincc columns adaptation.png" the columns marked on yellow is the data that I am importing. But not all the tags are being saved with the "start value" value accordingly. Log file is not that helpful! *** NOTE: All internal tags declared as WString are 255 in length. Start value on designer shows 128 length max. Could this be an issue when I am trying to import long texts?
Attachmentscreenshots.zip (661 Downloads) |
10/21/2021 4:20 PM | |
Joined: 2/19/2016 Last visit: 7/30/2024 Posts: 8 Rating: (0) |
I know this was an old post, but what was the resolution to this? |
Follow us on