5/31/2014 10:40 PM | |
Joined: 4/21/2006 Last visit: 9/17/2024 Posts: 510 Rating: (24) |
New question was splitted to a new thread: Migration from ProTool to WinCCflexible: Internal Server Error |
11/23/2015 2:05 PM | |
Joined: 5/26/2011 Last visit: 8/5/2024 Posts: 456 Rating: (7) |
Hello experts, This has been a very helpful discussion. I'm having trouble though on migrating a supposed to be OP7 protool project to WinCC Flex 2008 SP2 (reading the manual it's supposed to be finely migrated to OP77B). It says "no conversion available for this device" and "an error ocurred during configuration checking". I haven't opened the project myself since I don't have protool (if anyone can also help how I can get one, I'll really appreciate). So attached is a sceenshot and even the protool project. Thanks! AttachmentOP7 Migration Error.rar (609 Downloads) |
11/23/2015 5:57 PM | |
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: WinCC flexible 2008 Migration |
Eng.Mohamed Ibrahim |
|
11/23/2015 5:59 PM | |
Posts: 8946 Rating: (999) |
This are very old ProTool projects... I don't know if it makes sense to use the converted files... Anyhow, find this link https://www.sendspace.com/file/wnm8yx for WinCCflex OP177B converted files Silo 6 + Silo 7. |
Follow us on