Industry Online Support
Technical Forum
7/30/2013 2:56 PM | |
Posts: 8 Rating: (0) |
I have several HMI projects built on WinCC Flexible 2008 SP3. This program is installed, licensed and working on my PC under Windows XP Professional 2002 SP3. I have just installed Step7 Basic V12 on the same PC with a view to converting an OP177B project to use a KTP600. The main system is installed, licensed and working. However installation of the WinCC migration module of Step7 fails. The log file (attached) indicates that it was unable to find the SQL server. However Microsoft SQL Server 2005 is present and WinCC continues to work normally. I have removed WinCC, Microsoft SQL server and Microsoft SQL Native Client, rebooted and rerun the installation of WinCC Flexible 2008 SP3. WinCC still works and the Step7 installer still fails in the same way. Am I doing something wrong or missing something? Is there any way of working around this problem short of retyping the project from scratch? Attachmentlogfiles.zip (306 Downloads) |
Follow us on