9/27/2011 12:47 PM | |
Joined: 1/17/2007 Last visit: 3/8/2024 Posts: 1541 Rating: (531) |
Misuse of the private message facility. I have started to get a number of requests for help / assistance via private messages. Have my my fellow experts also noted this? Users should not use the private message facility for this purpose for the following reasons. 1) It is not what the private message facility is provided for. 2) It limits the advice just to one expert / user. Why limit yourself like this? Surely it is better to get advice from a number of experts / users, as it is not always certain that one person will know the answer. 3) It prevents other users from the benefit of seeing the problem and solution. Thus this means that other users cannot search for a answer to a similar / same problem and so have to ask the question again. 4) If that expert is away (at site, on holiday etc.) then it may take longer for you to get a reply. Splitted from Tips&Tricks for the forum usage. |
Last edited by: O_Moderator at: 10/10/2011 1:53 PMnew subject after splitting Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to20 thankful Users |
9/28/2011 9:44 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Hello together, if you get private messages from other users which you want to be imported by us (=Import-User-1) please send them to CS Moderator. We will then publish this question and iform the user which asked the question about it. I think this is the best way to handle with these questions, because they are then open for everyone and the community can see them and maybe the discussion will also help other users. Best regards O_Moderator |
This contribution was helpful to11 thankful Users |
Follow us on