5/17/2010 9:07 PM | |
Posts: 116 Rating: (7) |
Hi Berg, to control the axis you can use - commands of PLC open or - commands of the technology library(see technology - drive axis - motion - e.g. _move) If you use MCC you have a graphic library. I think you should start with this. It is possible to convert MCC programs to ST. (so you cansee how to program this in ST). MCC uses commands from the technology library. Maybe this FAQ will help a little bit http://support.automation.siemens.com/WW/view/en/27774657 Moreover you'll find a sample on the SCOUT DVD --> see Utilities&Applications \Utilities_Applications\SRC\5_EXAMPLES\ForBeginners\D435 \Utilities_Applications\SRC\5_EXAMPLES\FirstSteps Regards Jerry |
This contribution was helpful to1 thankful Users |
Follow us on