11/25/2009 7:49 PM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Dear Kthalji, Please check the following data copied from the manual:
Cause Motor power (P0307) does not correspond to the inverter power (r0206) - Motor lead short circuit - Earth faults Diagnosis & Remedy Check the following: - Motor power (P0307) must correspond to inverter power (r0206). - Cable length limits must not be exceeded. - Motor cable and motor must have no short-circuits or earth faults - Motor parameters must match the motor in use - Value of stator resistance (P0350) must be correct - Motor must not be obstructed or overloaded - Increase the ramp time - Reduce the boost level Also Please tell us more about your application, control method, and tell us the current of motor written on its name plate, current you have put in P0307 and then put p0005 = 27 [output current] and tell us the actual current value. Regards, |
Ayman Elotaify |
|
Follow us on