5/19/2020 5:34 AM | |
Posts: 19 Rating: (0) |
Scorp, I made a new test (see attachment), exactly as you told me, using the example I made for creating a LOGO! as Server and Computer as Client connection, In here the computer has the IP address 192.168.0.4, and the LOGO! has 192.168.0.2, both have the same subnet mask, and I used the program that you told me (to avoid using the other one), in this I don't know how to change the port so I leave it as 502. Still no connection, can you please try it on your LOGO! to see if it works? I added the LCD of my physical LOGO! where it says the MODBUS is Disconnected. Do you think that the local port and the Rem. Port should be the same? and that is the problem? Otherwise I have no Idea!! And its driving me crazy haha! AttachmentNewTest.zip (178 Downloads) |
5/19/2020 5:55 PM | |
Joined: 2/22/2008 Last visit: 5/10/2024 Posts: 2698 Rating: (206) |
Which Logo exactly do you have, order number and firmware version ? |
5/19/2020 6:10 PM | |
Posts: 19 Rating: (0) |
This one! |
Follow us on