6/19/2014 12:23 PM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Dear nicer, you're not giving up easily, I like that I don't know your capabilities but you should stick to solutions you are able to handle. There is no use of providing you with other possibilites if you strugglelater to implement them.
http://www.matrikonopc.com/opc-drivers/1603/index.aspx
http://hilscher.com/products_list_group.html?upg=15&pg=22
Best Regards. |
Give us your feedback and show us your respect! |
|
6/20/2014 4:56 AM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
1) Ok I would try your suggestion of trying the demo version even my software and hardware is older than the suggested compatibility. 2) Yap, I guess OPCs is another possibility, but it sound complicated to me and I'm sure it wouldn't be far cheaper if it would be cheaper at all. But one advantage would be it's not only the MODBUS TCP, but there will also be a range of other communication protocol that will be enabled. 3) I don't see replacing gateway would help, since the problem is the gateway driver itself. But I guess I should just see this as a remote option. 4) If 1 fails, this I guess sounds the best and simplest option to me (though I doubt for better integrators like you). I didn't know until now that there's already an included MODBUS TCP driver on the TIA Portal library for S7-1200, and since S7-1200 is cheaper than S7-300, that would be doubly better! I just wonder why there's a free library for the 1200 while there's not on the 300.. Anyways, thanks a lot for your continuous response! I would also like to invite you to also help me on this sub-thread:/tf/WW/de/Posts/110034#top Thanks again!
|
6/20/2014 9:12 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Hi nicer , On TCPdifferent terms are used compared to Serialbut meaning the same. Modbus-Serial Modbus-TCP Master=Client Slave= Server So your Schneider Gateway ison the serial side a Modbus-RTU Master to yourPower Meterswhich are the Modbus-RTU Slaves. At the same time the Gateway is at the TCP side a Modbus-TCP Server to yourS7-1200 whichwill be theModbus-TCP Client. So you need to configure a Modbus-TCP Client on your S7-1200. Best Regards. |
Give us your feedback and show us your respect! |
|
6/20/2014 9:32 AM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
I see. So on MODBUS TCP terms, a Client (S7 CPU) would be having many Servers (e.g., gateways) as the Profibus Master have many Slaves? What about my inquiry about the programming/configuration on the gateway side (server)? Thanks for your continuous response!
|
6/20/2014 10:39 AM | |
Joined: 12/1/2009 Last visit: 3/31/2024 Posts: 672 Rating: (147) |
Hello nicer, That gateway needs to be configured but how and by whom I cannot tell you.In case you need to do that you will have to study the gatewaysand PM's documentation. Best Regards. |
Give us your feedback and show us your respect! |
|
7/10/2017 1:13 PM | |
Joined: 6/19/2017 Last visit: 4/19/2024 Posts: 7961 Rating: (162) |
New question published by AutoGen_7545441 is split to a separate thread with the subject CB 1241 RS 485 communication board and 6 power meters: Communication is in good condition but in scanning data from power meters it goes wrong. Best regards |
My Forum is the place to personalize your profile, |
|
9/8/2017 8:49 AM | |
Joined: 8/21/2014 Last visit: 4/19/2024 Posts: 949 Rating: (13) |
New question published by AutoGen_530013 is split to a separate thread with the subject Using CPU412-5H redundant system for modbus communication without any CP card. Best regards |
Last edited by: Jen_Moderator at: 9/19/2017 1:01:14 PMInserted right headline. My Forum is the place to personalize your profile, |
|
Follow us on