5/13/2015 12:57 PM | |
Joined: 3/25/2012 Last visit: 2/16/2024 Posts: 99 Rating: (3) |
Also added the prg. Back-up. 3rd party device IP address 192.168.0.25 and CPU address 192.168.0.1
AttachmentMODBUS_P.rar (888 Downloads) |
This contribution was helpful to1 thankful Users |
5/16/2015 12:02 PM | |
Joined: 3/25/2012 Last visit: 2/16/2024 Posts: 99 Rating: (3) |
Hi kaulquappe Thanks for reply. 1)Defined IM151-8 as client by using Siemens ex. program. IP address is 192.168.0.30 2)Set the IP address 192.168.0.1 for 3rd Party device, this is the only thing i have to do on that side 3)For A100 checked the ip address on both side its ok. I dont know where i have to check the port No. ? communicated that server with MODSCAN software that is working well. after that i am trying with IM151-8 still connection_established= True is not coming. I am confused. i dont know where i am doing mistake please check the attached file and guide me. AttachmentModscanfiles.rar (719 Downloads) |
5/16/2015 12:06 PM | |
Joined: 3/25/2012 Last visit: 2/16/2024 Posts: 99 Rating: (3) |
`Attached the program also.
AttachmentPrg_backup.rar (728 Downloads) |
5/16/2015 1:33 PM | |
Posts: 3093 Rating: (322)
|
Hello SRITN, Regards, |
Follow us on