3/15/2017 4:57 PM | |
Posts: 439 Rating: (108) |
Hello, I will give more information than less. I have an IOT 2040 and a S7-1200. 6ES7647-0AA00-1YA2 SIMATIC IOT2040 6ES7 212-1AE40-0XB0 CPU 1212C DC/DC/DC I already tried the S7 node to communicate with the S7-1200, works perfectly. I am now trying to communicate via Modbus TCP, in case I have to communicate with a third-party device with Modbus TCP. I import the nodes "node-red-contrib-modbus 1.0.8" into my Node-Red. https://flows.nodered.org/node/node-red-contrib-modbus I am now able to add the "Modbus read" into my web interface. I am able to read the data from my S7-1200. I would like to manipulate the data received and only have the data value. Here is the format of data I receive when I specify I want only one variable:
I copied and paste the "Debug" output: Here are the current value in the DB of my S7-1200:
So, I would like to separate every variable in the DB and get the value only in the "msg.payload". Here is the data i receive when I specify i want 4 variables:
I tried "Split" and "Swich" node, but can't find a way to delete extra stuff.
Maybe a Javascript, but I am new to this... Any advice? Best regards, Hugo |
4/6/2017 7:23 AM | |
Joined: 2/27/2014 Last visit: 9/4/2024 Posts: 689 Rating: (200) |
Hello Hugo D, Can you provide some screen shot /Videofor configuration of Modbus TCp connection in IoT? When i am trying to make connection between S71500 PLC and ToT2040 over modbus TCP then i am getting error that "typeError : Cannot read property 'close' of null" and "typeError : Buffer.alloc is not a function". |
With Best Regards, |
|
6/22/2017 12:59 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by JasonChen37111 is split to a separate thread with the subject Problem when install node-red-contrib-modbus. Best regards |
6/28/2017 9:02 AM | |
Joined: 2/27/2014 Last visit: 9/4/2024 Posts: 689 Rating: (200) |
hello, Attached video is self explanatory. TCON_IP_V4 Interface ID is hardware id of PLC PN port=64 ID is connection id basically for serial communication (1...254)=1 Connection type is TCP =11 0r B ActiveEstablished is false so client can establish communication= 0 Remote address as partner IP address (IOT2040)=192.168.200.1 Remote Port=0 Local Port=502(Modbus TCP server port )
AttachmentMODBUSTCP.zip (538 Downloads) |
With Best Regards, |
|
6/29/2017 3:14 PM | |
Posts: 215 Rating: (6) |
Is there any way to read real or bollean values? Or am I limited to using integer and words? |
6/29/2017 4:55 PM | |
Posts: 439 Rating: (108) |
https://en.wikipedia.org/wiki/Modbus Coil Read-write 1 bit Discrete input Read-only 1 bit Input register Read-only 16 bits Holding register Read-write16 bits |
This contribution was helpful to1 thankful Users |
Follow us on