3/24/2020 6:12 PM | |
Posts: 34 Rating: (0) |
Hello! I need Project Sample of Modbus TCP configuration Through CPU PNIO - CPU315 Thank You.. |
3/24/2020 8:15 PM | |
Joined: 10/3/2008 Last visit: 4/6/2024 Posts: 954 Rating: (123)
|
Hi, the example projects are installed with the setup: https://support.industry.siemens.com/cs/ww/en/view/109745187 (current version). https://support.industry.siemens.com/cs/ww/en/view/109752686 (previous version) Wüstenräuber |
This contribution was helpful to3 thankful Users |
3/26/2020 2:11 PM | |
Posts: 34 Rating: (0) |
Hi Expert, I totally agree with You, The only conflict with me is That why Length=5 in The example? Thank You |
3/26/2020 10:17 PM | |
Posts: 34 Rating: (0) |
Hi Expert, I've uploaded a sample project I which I have downloaded to CPU-315-2-PN/DP simply I created on TCP connection to Communicate to Remote Slave IP (192.168.1.11) through Holding Registers (Saved in DB11) Starting From address 0 to 6 I have only Error A090 (That's because I don't have a licence). But in The same Time Connection not established yet!! Could you check the program Thank You AttachmentMODBUS_PN_CPU315-2.zip (382 Downloads) |
Follow us on