1/16/2020 3:18 PM | |
Posts: 11 Rating: (0) |
I connected new plc to the bus and i can see it and old plc on the pc. Still dont see lift bord, ill leave here my program for modbus on plcs its lbr for port 1, when i make same one for port 0 in onother program it wont work, its not connected to hmi or anything, when i program port 0 for modbus i use port 1 to download program. ill post all instructions i have for bord and how does it look like AttachmentNewZip.zip (398 Downloads) |
Last edited by: AlexProSparks at: 01/16/2020 15:19:27 |
|
Follow us on