11/23/2015 2:51 PM | |
Joined: 2/28/2015 Last visit: 5/30/2022 Posts: 9 Rating: (0) |
Hi, As manual says: "When the -> safety program is started, all data blocks with -> F-attribute are initialized with values from the load memory (as with a cold start). This means that saved error information is lost" So, if we change some value (i.e limit switch value) in F-DB during machine work, after power reset all values will be reset to values from last program download. Is there any way to change this value without downloading F-DB again? I would like to give to operator possibility to change this value, but this value has to be retianed. I think that maybe "FC 178 "F_INT_WR": Write Value of Data Type INT Indirectly to an F-DB" can do it, but I dont have possibility to check this. However I have to plan how to solve this issue. Regards Daniel |
Follow us on