2/22/2011 11:21 AM | |
Posts: 2348 Rating: (263)
|
Guess you need "(" when you call SFC51 :^) |
2/22/2011 11:28 AM | |
Posts: 84 Rating: (19) |
helloAret i didn't understood what u said about... hope u understood my problem thanks
|
2/23/2011 6:22 AM | |
Posts: 84 Rating: (19) |
Thank you very muchChilly_GarfieldandAretfor helping me out.... i am now studying over the program. wish to get more support on making a program to fetch CPU and I/O module faults to SCADA.. Thanks again.. |
This contribution was helpful to2 thankful Users |
4/20/2015 2:16 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Please have a look at this : Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x) A simple possibility for an evaluation of the diagnosis of distributed I/O modules in connection with SIMATIC S7 is needed. The diagnostics evaluation is done both for PROFIBUS DP master systems and also for PROFINET IO systems. https://support.industry.siemens.com/cs/in/en/view/98278878 Components of the diagnostic package PNIODiag
This documentation explains the structure of the data of the system and station diagnosis in the two data blocks in the diagnostic package PNIODiag, which allows you to evaluate and process the system and station statuses in the user program, the diagnostic package PNIO determines and displays in the visualization. Function Block FB126
Visualization Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on