5/30/2009 10:18 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello kumar, I think the best choice for you is "RSE" or what we call "Report System Error" Siemen offers this option for Simtic Manager Ver. 5.4. With the Report System Error function, STEP 7 offers a convenient way to display diagnostic information supplied by the component in message form.. The necessary blocks and message texts are automatically generated by STEP 7. All the user has to do is load the generated blocks into the CPU and transfer the texts to connected HMI devices.
I think this way is a very easy way to diagnose modules and also to display diagnosis on your HMI. To display RSE messages on HMI, few settings should be made in WinCC flexible as here in this link. How can you have system error messages from a SIMATIC S7-300 / 400 displayed in WinCC flexible? I hope this helps. Best Regards |
Last edited by: Ayman Elotaify at: 5/30/2009 10:20 AMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
6/1/2009 7:29 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hi saravana kumar, Look at How can you report S7 system errors in WinCC? Also How can you configure the "Report System Error" functionality of an S7 station to be multilingual? Or give more details about what exacly you already done. Hope this will helps. Best regards Hristo Mihalev |
This contribution was helpful to1 thankful Users |
6/3/2009 7:58 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello saravana kumar, But did you received "correct" errors in Simatic Manager when you test the CPU messages? regards |
6/3/2009 8:03 AM | ||
Joined: 2/6/2009 Last visit: 4/29/2024 Posts: 938 Rating: (118) |
Yes I have checked in the Diagnostics Buffer and it was giving all errors. |
|
Last edited by: saravana kumar at: 6/3/2009 8:04 AM_______________________________________________________________ |
||
6/6/2009 1:58 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Dear Kumar, have you followed all instruction to implement the RSE in WinCC? Regards, |
Ayman Elotaify |
|
Follow us on