Industry Online Support
Technical Forum
3/19/2009 7:13 AM | |
Posts: 325 Rating: (13) |
Hi All, This perticular project was developed by my colleague on his laptop. The configuration has as 417H-System and Simcodes. On his laptop, its giving Zero Errors. Later when the same project was Archieved and Retrieved on my laptop, its giving 60 errors during CFC compilation and all these errors point to the following message "The CPU_DIAG parameter at block SIMOCODE_pro_C11 of type MOD_PAL0 is not available.". Find enclosed the error log attached. Need some help to resolve this!!!!!!!! Regards Nil AttachmentSIMATIC H Station_1__Module driver.pdf (127 Downloads) |
3/19/2009 12:06 PM | |
Posts: 433 Rating: (48) |
Hi Nil96, the block MODB_PAL0 is a part of the PCS7 library. Do you have installed the same PCS7 version on your laptop like your colleague? Tomcat |
Follow us on