7/5/2018 6:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Which is the Bus module? Please refer attached sheet for BM & IM compatibility issue. HTH. |
7/5/2018 4:25 PM | |
Posts: 56 Rating: (1) |
I am using the normal bus connector 6ES7 390-0AA00-0AA0 |
7/6/2018 1:37 PM | |
Posts: 56 Rating: (1) |
Address on the DIP switches are correct and i've tried to cycle the power several times with no success of getting it to work |
7/8/2018 7:16 AM | |
Posts: 56 Rating: (1) |
Hi I am not using any Active bus module all the modules are connected via 6ES7 390-0AA00-0AA0 bus connectors My setup consists of 1 interface and 3 I/O modules |
7/16/2018 12:36 AM | |
Posts: 56 Rating: (1) |
After upgrading to Step 7 V 5.6, i am now able to find the part "153-2BA10-0XB0" but now i got this BUS Fault and SF Fault, will send the Buffer data soon |
7/16/2018 6:00 AM | |
Joined: 7/27/2016 Last visit: 8/16/2023 Posts: 17 Rating: (0) |
Go back to 5.5 SP4 and get the HSF from June, also get the HF12. |
7/16/2018 6:51 AM | |
Posts: 56 Rating: (1) |
Hi landlord323 Please can you put in some more details... Thanks in advance |
Follow us on