4/15/2016 4:00 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello Pasanna, I have two ideas about that. I can't test it right now, but it looks promising. If I understand the manual (https://support.industry.siemens.com/cs/ww/en/view/109096785/36127127307)
You can find the syntax and a description if you click on the property. Alternatively if you select the "memory space view" element in your screen and go to "Properties > Animations > Tag connections" you can add a tag (Integer). I'm not sure though weather this is read/write. This might not work in simulation. I would try it on a running runtime. Once you read the integer value you can convert the data type to a string, if you want to use "text". PS: Next time please state in your opening post which runtime you are creating the project for. In this case WinCC RT Professional (and the version including at least the servicepack version (V13 SP1?)). |
Last edited by: H.J. at: 4/15/2016 4:02:35 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to2 thankful Users |