1/5/2020 10:48 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello. I am looking for some guidance to what i thought would be a straight forward solution to a problem. conveyor system...is chain a driven system with carriers attached 150mm apart. Product is hung from the carriers. Counting the product on each carrier is straight forward but I am trying to count the missed product for example if the operative has not placed the product onto the carrier i need the means to count that. I have attached my test program, my problem seems to be the gap between each carrier as you will see from the attached file. I inverted the counter blocks pins to try to use the gap but all i am doing is picking up the gap between the carriers and not the missing product hope someone can point me in the right direction. Ade Attachmentmissed_product_test.zip (141 Downloads) |
1/6/2020 1:28 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Thank you, back to the drawing board for me Ade |
1/7/2020 7:37 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32882 Rating: (4065)
|
If the first product is already missing, no monitoring time can be started ... |
1/7/2020 8:46 PM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, Thank you for taking time out to help me, I will implement you solution into a live test Ade |
Follow us on