2/21/2018 10:45 AM | |
Joined: 5/20/2015 Last visit: 6/29/2022 Posts: 6 Rating: (0) |
Hello Huggy, I found that you can see how many connection are made in the 1500 PLC. For example, my project makes 12 connections, the NCM S7 diagnostic tool could show me the amount of packages being send/received through that connection. The functionality that I'm looking for is monitoring the amount of packages send/received through the connections (not in total but for each connection) Greetings, Engjell ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/21/2018 2:04:45 PMNew subject after splitting |
|
2/21/2018 6:06 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15204 Rating: (2417)
|
I am not saying this does not exist in TIA Portal. I am only saying that *I* do not know anything about that type of information within any blocks provided with TIA Portal. There may be an add-on optional set of blocks Siemens provides. Or, it may be I am not thinking correctly about using the provided tools to figure out the count values you are talking about. I do know we can access some generic data from the PLC. One of them is communications statistics. I know this because TIA Portal displays those statistics in certain situations. However, I do not know if that is sufficient for your needs. If that is what you want, you would have to search the forums / web site for the correct DPRD_DAT parameters to retrieve it. I do not recall when this information was posted, but the search tools and your existing knowledge about older system designs should get you there quickly.
|
science guy |
|
Follow us on