1/22/2016 4:56 AM | |
Posts: 87 Rating: (0) |
Hi, I have a problem with Motion Control Master Drive and Servo Motor with Resolver. The specification of Master Drives and Motor: MASTERDRIVES MC AC/AC DRIVE 6SE7022-1EP50 The Parameter file (Drive Monitor) is attached. MOTOR: 1FK7086-7SF71-1SG2 RESOLVER p=4 N03 The last motor was broken. So we replaced with the new one. The problem is the motor rotation is reverse. If we change the terminal U-V-W on MasterDrives, the motor is abnormal. Hope someone have experience about this case. Is recommended to change / rotate encoder position? Thank you, Best regards, Sasongko AttachmentTaglio_NR231.rar (264 Downloads) |
Follow us on