Industry Online Support
Technical Forum
11/29/2012 3:25 AM | |
Joined: 11/23/2012 Last visit: 10/20/2020 Posts: 6 Rating: (0) |
I am new to S7 1200 and just trying out Motion Control. The problem I have I cannot seem to get it to Commission using the interface in the TIA. Attached are the screen shots. The error I get is that it keeps saying the parameters are not correctly set in the Axis Object, but when configuring the block prior to commissioning, the settings all get a blue or grren tick. Using V11 Basic ( not yet upgraded to P1 or SP2 as the VirtualBox framework the S7 Basic program is laoded into, hasn't got the memory to allow an upgrade). PLC is 1214C Ver 1 (I think). I have tried leaving the Select "Enable Output" box blank, as I cannot decipher anywhere in Siemens manuals etc what this is for Any ideas? AttachmentMotion Configure Problem.zip (141 Downloads) |
Last edited by: O_Moderator at: 11/29/2012 12:21 PMnew subject after splitting from /tf/WW/en/Posts/31842#top |
|
Follow us on