3/29/2013 3:04 PM | |||||
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello Karnan: One suggestion: try the search box at the right to locate equipment for which you already have part numbers. Had you tried this with your motors MLFBs, you would have found these links to Product Support: (try it!):
Within these links you would have seen this manual for the 1FK7 motors: SIMODRIVE 611, SIMOVERT MASTERDRIVES MC, 1FK7 Synchronous Motors Dimensional drawings are available in chapter 6 of the manual. Look at the attached file for an example. Hope this helps, |
||||
This contribution was helpful to1 thankful Users |
4/11/2013 5:50 PM | |
Posts: 767 Rating: (69) |
Hello Karnan, Another very useful tool for this information is to use CAD Creator, which is a website tool to be access drawings for any of these types of motors. The tool can be accessed in two different ways: 1. Following address: http://staging04.it-motive.de/CADCreator/VorNavigation.cfm?IdListVornavi=(0-1*906)&CFID=2963806&CFTOKEN=26348610&Scenario= 2. Use Google search engine by entering "CAD CREATOR" and similar choice will be shown to above on first page from my experience. Once CAD CREATOR is initiated copy and paste entire part number in the search window box located in upper right corner of screen. Then choose Synchronous Motor button located in middle of screen. Note: If motor desired would be a geared motor then choose Geared Motor button. Alternatively, if complete part number is not known yet (or not available to copy and paste) may use Product Choice Navigation Tree located on left side of display. Expand the specific SIMOTICS motor line according to match of the first four digits of part number (for instance "1FK7"), Choose "Order Number" then build part number using pull down menus for each digit. Once part number is built drawings are available in many different formats: 2D (must enter email address) 3D (must enter email address) Best Regards, Deputy |
This contribution was helpful to1 thankful Users |
Follow us on