8/8/2019 12:42 PM | |
Joined: 6/24/2013 Last visit: 4/22/2024 Posts: 1588 Rating: (409)
|
Hi 1.make sure drive is configured to use profibus and right process image etc. is used 2. Example of drive control (STEP 7 project, FC140 is a servo control) attached. the FC which controls the drive can be re-used in your project note: attached exampole is a cut-down project (removed irrelevant items to make it small) AttachmentSew_driv.zip (501 Downloads) |
Last edited by: Piotr.M at: 08/08/2019 12:42:37 |
|
This contribution was helpful to1 thankful Users |
4/27/2022 8:59 PM | |
Joined: 11/12/2015 Last visit: 2/22/2024 Posts: 17 Rating: (1) |
SEW_Sample_TIA_S7300_Movilink_Param_V2.1.zip - TIA V14 This TIA sample project is to illustrate the parameter access regarding various SEW PROFIBUS DP-V1-slaves or PROFINET IO devices. The project focuses on function block FB100 "DS47_Parameterhandling" _____________________________________________________________ Program structure: OB1, OB1/NW1: CALL FC100 "MOVIDRIVE_&_FB100": /NW2: CALL FC102 "MC07_Gateway_&_FB100": FC100/NW1: "MOVIDRIVE_&_FB100": Reading the Variable H0 FC102/NW1: "MC07_Gateway_&_FB100": Writing the fixed setpoint N11: PROFIBUS DP-V1-Master / PROFINET IO-Controller I I PROFIBUS DP / PROFINET IO I Gateway DFx (DFP21B, DFE32B,..,..) I I SBUS I_______________________..... MC07_1 MC07_2 MC07_3 SBUS-Address = Sub address More detailed information can be found in the program itself. This sample program only demonstrates the basic approach. We do not accept legal or other liability for incorrect program functions and their consequences! Status 2.1; Mai 2020 SE-PAS SEW-EURODRIVE GmbH & Co KG AttachmentSEW_Sample_TIA_S7300_Movilink_Param_V2.1.zip (323 Downloads) |
Last edited by: Barsukovm at: 04/27/2022 21:10:09Last edited by: Barsukovm at: 04/27/2022 21:26:57 |
|
4/27/2022 9:05 PM | |
Joined: 11/12/2015 Last visit: 2/22/2024 Posts: 17 Rating: (1) |
SEW_Sample_TIA_S71200_MOVILINK_Param_V2.1.zip - TIA V14 PROFIBUS AND PROFINET EXAMPLE This TIA sample project is to illustrate the parameter access regarding various SEW PROFIBUS DP-V1-slaves or PROFINET IO devices). The project focuses on function block "Par-FB100" (FBD) and "Par-FB111" (SCL), they control data set 47 (PROFIdrive). Both FBs have the same functionality and interface. _____________________________________________________________ Program structure: OB1, OB1/NW1: CALL FC100 "Par-FB111": FC100/NW1: Reading the variable H0/MOVIDRIVE NW2: CALL FC200 "Par-FB100" FC200/NW1: Writing the fixed setpoint N11/MOVIDRIVE FC200/NW2: Parametrize the Modulation frequency = 16 kHz; Gateway-application with MOVITRAC PROFIBUS DP-V1-Master / PROFINET IO-Controller I I PROFIBUS DP / PROFINET IO I Gateway DFx (DFP21B, DFE32B,..,..) I I SBUS I_______________________..... MC07_1 MC07_2 MC07_3 SBUS-Address = Sub address More detailed information can be found in the program itself. This sample program only demonstrates the basic approach. We do not accept legal or other liability for incorrect program functions and their consequences! Status 2.1; May 2020 SE-PAS SEW-EURODRIVE GmbH & Co KG AttachmentSEW_Sample_TIA_S71200_MOVILINK_Param_V2.1.zip (259 Downloads) |
Last edited by: Barsukovm at: 04/27/2022 21:06:27Last edited by: Barsukovm at: 04/27/2022 21:08:28Last edited by: Barsukovm at: 04/27/2022 21:09:37 |
|
Follow us on