2/9/2012 8:54 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hello, You need to reflash the panel with the option 'Reset to factory defaults'. In that case ProSave will catch panel's bootloader and start to reflash panel at that point. It should help you 90% . Please read manual of MP277 on how to do it. SIMATIC HMI HMI device MP 277 (WinCC flexible)chapter 7.7.2. Also here What settings do you have to make on an MP 377 to reset the operator panel to the factory settings?. MP is different, but procedure is the same. |
Last edited by: Darius at: 2/9/2012 9:02 AMLast edited by: Darius at: 2/9/2012 9:00 AMBest regards, |
|
2/9/2012 10:30 AM | |
Joined: 12/13/2011 Last visit: 2/13/2024 Posts: 145 Rating: (6) |
the imagesare hostedhere |
4/19/2012 1:11 PM | |
Joined: 2/13/2012 Last visit: 9/16/2018 Posts: 16 Rating: (0) |
How to do that? because my HMI hang on "Startup in progress". Please explan procedure. I have MP377 15" touch same problem. Sometime hang at partition 0 and sometime hang at partition 1. |
4/19/2012 1:21 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, See 2nd Link Darius posted. Regards, Marcjan |
Problem solved? |
|
4/20/2012 4:15 AM | |
Joined: 2/13/2012 Last visit: 9/16/2018 Posts: 16 Rating: (0) |
2nd link need boot up complete. but now it not complete. Cannot do everything only ping |
4/20/2012 7:12 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, In case of this panel in warenty period, please call your seller or local Siemens representative to replace it.
|
Ayman Elotaify |
|
4/20/2012 7:24 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, Here are the steps:
If that doesn't work you have to send the Panel for repair Regards, Marcjan |
Problem solved? |
|
Follow us on