Industry Online Support
Technical Forum
11/3/2008 10:23 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, did you have try this name "Administrator" "100" regards, |
11/5/2008 10:33 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, you can change the user name and the password. I have also every time problem to see where can i found the parameters to change somethink. So i have made know a "manual" (for me). Maybe you can also using this info. AttachmentPic_Service.zip (270 Downloads) |
Last edited by: The Brain at: 11/5/2008 10:34 AM |
|
11/11/2008 2:34 PM | |
Posts: 95 Rating: (0) |
Dude! thanks:) I will use it as I have two customers currently wanting to utilize this feature. There are two options for remote access to an HMI, smart service and smart access. I am not sure which I am actually using, I bought both options for my one project, but reviewing your images it seems like smart service is the option that allows remote control and changes. The option in the miniweb page for sm@rtclient is a part of which option? I assume smart service as this is how you access the miniwebpage from the HMI. I just want to make sure I understand what is needed. thanks again! John |
Follow us on