5/21/2012 9:45 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Hi, I suppose you've allready tried this What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? As long as your HMI is lets say 'dead', please power off it, configure Prosave as stated in that link, press 'Update OS' button and only the power on the HMI. If boot loader of HMI is still alive, you should be successful. Also, please make double and tripple check that you're using correct firmware version. Also, please tell me what do you see when power on the HMI ? Do you see any proof that bootloader is still alive ? It should stated at lest version of bootloader. If not, then I think you have big problems |
Best regards, |
|
This contribution was helpful to1 thankful Users |
5/21/2012 9:53 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello dipakkadam_619, Have you seen this FAQ? What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? how do you do an operating system update (OS update) on operator panels? if those FAQ doesnot help. use Support Request |
VANDE MATARAM..... |
|
1/6/2014 12:00 PM | |
Posts: 87 Rating: (0) |
Dear Macjan, How I can connect the MP 337 when it still bootloading process? As long as I know that we can connect in Windows system. Thank you |
1/6/2014 12:13 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168)
|
Hello Sasongko, Perhaps the following link might help: how do you do an operating system update (OS update) on operator panels? And: What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? Best regards, Wizard |
Last edited by: Wizard at: 1/6/2014 12:15 PM |
|
3/18/2014 2:54 AM | |
Posts: 87 Rating: (0) |
Dear Weirdooo, I have tried to factory reset with WinCC2008. I used straight Ethernet cable. It was work well. Actually, that was need much time until finished. |
11/5/2015 10:25 AM | |
Joined: 8/21/2014 Last visit: 9/17/2024 Posts: 1024 Rating: (14) |
New question published by Karthy is split to a separate thread with the subject Where can I find the IP adress of a device?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on