4/30/2015 7:38 PM | |
Posts: 1 Rating: (0) |
Hi, I am having comfort panel TP1200 with Siemens 315-2DP CPU. Earlier I was using MP377 with 315-2DP CPU on the MPI communication. Now i have choose comfort panel as MP377 is not available and migrated my project in to the TIA portal V12. Now my configuration is TP1200 with migrated project (from WIncc flexible to TIA portal) and S7315-2DP CPU programmed with step7 5.5 SP3. I am using another same system in other machine and communicate both the machines via MPI for some data exchange through X-GET. Some problems i am facing as below. 1. While all the MPI communication on 187.5 KBPS i observed that in one machine HMI, screen gets jump from one to other screen and i am not able to work on the HMI. And the other machine HMI is giving batch report print outs without running any batch and every time when i switch on the machine. 2. Due to screen jumping issue, I have changed MPI baudrate from 187.5 KBPS to 1.5 MBPS , in that case my screen jumping problem is solved but when the batch ends and report triggers, it prints continous batch reports without stopping and these reports does not contain any information which is required like actual alarms occured in batch etc. 3. I also tried and took both the machine on seperate PLC to HMI profibus DP connection and kept MPI connection only between both CPUs only to handshake, But still my batch report problem in point no.2 is not solved. But screens are not jumping now. 4. Also i observed that some times i see some happenings on HMI, like color change of valves and graphics, buttons get disappear for some time and appear again etc. 5. I also done "software rebuild all" for both the HMI's TIA softwares and also deleted \\flash\simatic folder and reloaded softwares again but could not find the solution. 6. Same kind of many systems are working well with MP377 and S7 315-2DP combination and there is no complains but when we start using comfort panel and TIA portal, we are finding this kind of problems. Requesting to suggest solution for the same. Best Regards, Jaykumar
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/4/2015 12:22:58 PMNew subject after splitting |
|
Follow us on