7/5/2013 10:37 AM | |
Joined: 10/20/2008 Last visit: 2/25/2024 Posts: 10 Rating: (0) |
Hi, i have made a MotionController in FB. i create an instance (DB104) in a FCand test it in Simu_mode, it functions oke. I call this one M1 Funtioning: Input = Start, Output = motor running. Working: when Start= '1' then motor starts running after 3seconds. When Start='0' then motor stops after 5 seconds when i create a next instance in the same FC (M2) then i use the Motor running as input. I asume that this instance wil then start after 3 seconds and stop after 5 seconds when the previous motor starts and stops. But that is not the case. The first instance is still working oke but the next one stops when the previous stops. When looking in the Instance DB i see the Delay-timer running for 5 seconds but the motor has allready stopped? Question: is this a Simulation Bug or ma i doing something wrong? AttachmentFB100.pdf (167 Downloads) |
Last edited by: O_Moderator at: 7/5/2013 10:47 AM |
|
7/5/2013 10:51 AM | |
Posts: 1064 Rating: (72) |
are you using the same data block?? |
7/5/2013 10:53 AM | |
Posts: 8946 Rating: (999) |
Hi Wizzard, why? That part is not neccesary, I think. |
7/5/2013 11:00 AM | |
Joined: 10/20/2008 Last visit: 2/25/2024 Posts: 10 Rating: (0) |
Hi, Yes, i am using the same instance of FB100. I just seen that it is not only when stopping but also when running. regards, Wim. AttachmentFC101.pdf (134 Downloads) |
Last edited by: O_Moderator at: 7/8/2013 10:32 AMattachment reattached Last edited by: Wim_ at: 7/5/2013 11:09 AM |
|
7/5/2013 11:35 AM | |
Joined: 10/20/2008 Last visit: 2/25/2024 Posts: 10 Rating: (0) |
second |
Last edited by: O_Moderator at: 7/5/2013 11:58 AMattachment reattached |
|
7/5/2013 11:50 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, Do you use your SFB with multiple instance capability? How do you create and update multiple instances? using SFBs in FBThe issue with the monitoring is normal when monitoring Bigger blocks or multiple networks.Regards, Marcjan |
Problem solved? |
|
Follow us on