10/18/2016 9:59 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating: (45)
|
Hello , you can use PDM for the connection / communication. Simatic PDM 9.x single point for the communication ==> 6ES7658-3HA58-0YA5 Modbus Cable for the connection ==> 7ML1830-1MC Here you will find a guide ( made for PDM 6.x which is similar to 9.x) ==> http://www.automation.siemens.com/w1/efiles/feldg/files/application_guides/en/ag041125.pdf Also this blog is interesting: Hope this helps ! |
This contribution was helpful to1 thankful Users |
11/16/2016 7:01 PM | |
Posts: 32 Rating: (2) |
Thanks! What is the infared link 7ML1830-1MM? Would it allow PDM usage through the infared port, instead of opening the box to connect to the RJ connector?
|
Last edited by: cncsparky at: 11/17/2016 4:45:07 PM |
|
2/22/2017 9:14 PM | |
Posts: 32 Rating: (2) |
Modbus Cable for the connection ==> 7ML1830-1MC Is there an alternative to the Siemens cable? Cost on this one is around $1000 !! The PDM was less than $100. |
2/23/2017 11:44 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating: (45)
|
I have double checked this.The listprice of 7ML1830-1MC will be around 70 $. Who gave you a price of 1000 $ ??? |
2/24/2017 8:07 PM | |
Joined: 3/28/2010 Last visit: 9/18/2024 Posts: 1056 Rating: (213) |
Which port are you connecting to? RS-232? RS-485? The RS-485 connection at the MultiRanger is screw terminals. There is no need for a 'cable' because the cable is shielded twisted pair connected to screw terminals. The RS-232 connection is an old style RJ-11 or RJ-12 telephone connection. There are inexpensive 4 conductor or 6 conductor (RJ-11 or RJ-12) cables with connectors on each end. https://s2.postimg.org/y7vuimfx5/rj12_6_P6_C_color_order_reversed1.jpg There are adapters that convert from RJ-11/12 to DB-9. The adapters have pins that are inserted in the appropriate DB9 shell to get the correct RJ cable conductor to the correct DB9 pin. One style has male pins, the other style has female sockets on the DB9 side. https://s13.postimg.org/u43llke4n/RJ12_DB9_F_adapter_crop_2.jpg In the US, the cables are about 3-4USD each, the adapters are about 3-4USD ea. I found this wiring diagram that I think if for the MultiRangers, but I have done this without 7 jumpered to 8 on the DB9 side: https://s1.postimg.org/s0emn4bhb/DB9_to_RJ_11_12.jpg |
Last edited by: danw at: 2/24/2017 8:07:35 PM |
|
Follow us on