7/8/2020 2:31 PM | |
Joined: 8/5/2016 Last visit: 3/11/2023 Posts: 1 Rating: (0) |
Do you have a copy of a working image file to be copied to the IC using the EEPROM writer. The IC number is Flash Memory number AT25DF321A HMI model is TP1500 Comfort Problem: We can't update OS of TP1500 Comfort from within Prosave V13.0.1.0 .It displays : No bootable device Please restart system. Checked the cross cable between the laptop and the HMI and chose reset to factory settings using the TP1500 MAC address shown on the back of the HMI.Also, used 3 different versions of TP1500 Comfort image files. The Prosave display is stuck on the laptop saying : Please boot the HMI device, and does not change by recycling power to the HMI TP1500 Comfort. We noticed also that the Siemens screen logo alternates with the message no bootable device , please restart system. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/08/2020 14:35:07New subject after splitting Last edited by: Adel Aly at: 07/14/2020 12:58:44 |
|
7/27/2020 6:43 PM | |
Joined: 9/14/2009 Last visit: 12/7/2023 Posts: 41 Rating: (0) |
Dear All i have same problem with comfort panel |
Follow us on