12/30/2013 11:17 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello Milosh, Which version of TIA Portal are you using? If you are using TIA Portal v12, it is more easy. In most cases, you will have to recompile and load the program after block access has been converted. Procedure To set the block access, proceed as follows: 1. Open the "Program blocks" folder in the project tree. 2. Right-click on the block whose block access you want to change. 3. Select the "Properties" command in the shortcut menu.The properties dialog box of the block opens. 4. Click "Attributes" in the area navigation. 5. Enable or disable the "Optimized block access" option. 6. Confirm your entries with "OK". For more info on this, check Basics of block access and Setting up block access. Let know if you are not using TIA Portal v12. |
Like it? Rate it! |
|
1/2/2014 9:39 PM | |
Joined: 8/16/2010 Last visit: 4/24/2024 Posts: 636 Rating: (12) |
Please share your solution... |
Follow us on