7/2/2019 2:52 PM | |
Joined: 7/6/2017 Last visit: 9/26/2022 Posts: 2 Rating: (0) |
hello to all I am trying to control Hydro Turbine using s7-1500 CPU. I cannot find the tracking of MW/GV OPENING as in the other DCS systems such as Emerson. can anyone be helpful to provide me the basic program to control the PID for the HYDRO governor. Thanks in advance Regards Rachit ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/03/2019 10:27:45New subject after splitting |
|
7/9/2019 9:27 AM | |
Joined: 4/28/2015 Last visit: 10/9/2023 Posts: 394 Rating: (55)
|
Hello, what do you mean with "MW/GV OPENING"? I'm sorry, but I can not understand your question... Maybe it will be helpful for you, to have a look at the distributed control system (DCS) of Siemens: SIMATIC PCS 7. |
7/17/2019 7:38 AM | |
Posts: 4 Rating: (0) |
hey MW/GV OPENING MEANS. MEGAWATT AND LOAD CONTROL SPEED CONTROL CAN YOU PLEASE HELP ME ANY REFRENCE PROGRAM OF THE SAME THANKS IN ADVANCE RACHIT |
7/22/2019 5:38 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello RAC_12345, the speed control can you implement with the blocks both blocks are part of the Advanced Process Library (APL). The APL is the standard library in PCS 7 where no additional licenses are needed. The load management blocks are part of the Industry Library (IL). The IL is an addition library in PCS 7, so you need additional licenses. With regards |
Follow us on