11/15/2018 9:52 AM | |
Joined: 5/14/2018 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Hi Owei, can you pls give me an example project of RF685R in pcs7 v9.0 Sp1 environment. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2018 2:17:07 PMRemoved E-Mail address, because doesn't comply with forum terms. Last edited by: Jen_Moderator at: 11/15/2018 2:18:07 PMNew subject after splitting |
|
11/22/2018 10:17 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Ben_Bene, you can find an example for RFID in the PSC 7 environment in the application example "Utilization of RFID systems in the PCS 7 environment". The Application example is vaild with PCS 7 V8.2 but it also works with PCS 7 V9.0 SP1. In the next time it should be available with PCS 7 V9.0. With regards |
This contribution was helpful to1 thankful Users |
11/22/2018 1:38 PM | |
Joined: 5/14/2018 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Hello Heisenberg, Thanks, do u have something with no MOBY connection. I need a direct profinet connection project. I believe it is the Ident Profile to be used, but I cant find a channel driver for it in PCS7 v9.0. Thanks in advance again! |
11/29/2018 8:28 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Ben_Bene, the application example is with PROFINET use an MOBY, but it's also valid with a dircet PROFINET connection. Here an short instruction:
For the instruction i merge the follow application example:
with regards |
11/29/2018 9:47 AM | |
Joined: 5/14/2018 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Hello Heisenberg, Appreciate the effort you made, but I had commissioned already the RFID, it is online now in PCS7. The only problem I have since the beginning is whenever I drag and dropped the ident profile in CFC I am getting error that array is not supported. this is the reason why I am looking for a driver that is compatible for PCS7 v9.0, or did I miss something here? Danke im Voraus! |
11/29/2018 10:22 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Ben_Bene, do you use the PCS 7 libary (4,2 MB) from the application example Utilization of RFID systems in the PCS 7 environment ? Because with this libary I can import and compile the CFC chart wihtout an error message. And I use PCS 7 V9.0 SP1. with regards |
Last edited by: Heisenberg2 at: 11/29/2018 10:23:13 AMLast edited by: Heisenberg2 at: 11/29/2018 10:37:21 AM |
|
This contribution was helpful to1 thankful Users |
11/30/2018 3:24 PM | |
Joined: 5/14/2018 Last visit: 4/25/2024 Posts: 6 Rating: (0) |
Hi Heisenberg, Thanks for highlighting the library part, I inserted it already in my project and tried to drag and drop the RFID driver and now it has no error anymore. My question is, the logical address of the RFID should be connected to the UDT Hw Connect right? If yes, then is it ok to use the UDT that is existing on the sample project that I downloaded from the link that you gave. To be exact it is UDT1900. I hope the connection of this UDT to FB2900 is not gone because I just copied the contents of the library to the Example project RF685R. Your support is much appreciated, thanks for the help as always. Schönes Wochenende!
|
Follow us on