Industry Online Support
Technical Forum
12/20/2009 8:25 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (308) |
Hello, All GSD for Simatic are available here: http://support.automation.siemens.com/WW/view/en/113652 I don't believ that the GSd is the problem, but rather that you have to configure your application in two different engineering tools (Step7 for Simatic, an the tool for AB). The number of bytes that will be exchanged must be configured on both sides. And any mismatch will empeach the slave to be configured in a right way by the master. |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on