2/19/2014 3:36 PM | |
Joined: 1/24/2014 Last visit: 3/13/2024 Posts: 119 Rating: (1) |
hello, if i post a complete little project for correction then can i get favour from Experts??? kindly tell me...
|
2/19/2014 7:27 PM | |
Joined: 1/24/2014 Last visit: 3/13/2024 Posts: 119 Rating: (1) |
hello, this is my first project after reading fourm and manuals. i made a simple ladder logic with Timer ON and S_pulse. and a simple input and output named as alarm in Network 5. i also made HMI for it.. please see my attachment in link after download. i display S_pulse time time after converting BCD to INT. and this is INT value run as this timer go run. but i want this time in seconds. secondly i need alarm sound in it...when input set then alarm sound should come out . and a message should highlighted(i.e my name.) 3rd can i put any picture like turbine in background with very rich graphics. please help me in this manners.this will help me much for better understanding. And please please tell me, how much this project can be improved that diferentiate me from others beginners. i put my great effort.waiting for good responce specially EXPERTS here. Attachmenttutorial.zip (88 Downloads) |
Last edited by: GrasserF at: 2/19/2014 10:49 PMdeleted Link, |
|
2/19/2014 7:58 PM | |
Joined: 1/24/2014 Last visit: 3/13/2024 Posts: 119 Rating: (1) |
dont take serious that line.. i am trying to become better with practice gradually... please...
|
2/19/2014 8:02 PM | |
Posts: 8946 Rating: (999) |
Good luck! |
This contribution was helpful to1 thankful Users |
2/19/2014 8:09 PM | |
Joined: 1/24/2014 Last visit: 3/13/2024 Posts: 119 Rating: (1) |
kindly download the the project from the link. and guide me , for my questions
|
2/20/2014 5:53 PM | |
Joined: 1/24/2014 Last visit: 3/13/2024 Posts: 119 Rating: (1) |
i am waiting for replies... |
Follow us on