1/25/2021 4:02 PM | |
Joined: 3/16/2020 Last visit: 11/6/2022 Posts: 5 Rating: (0) |
Hello I need to test the functionality of the SM1234 module's analog output (configured for voltage). According to the S7-1200 manual a value of 27648 should give me 10 V. This is true when I look at NORM_X and SCALE_X blocks. However my multimeter measurement reads -1.7V between terminal 0/0M and -12V between terminal 1/1M. I'm wondering if I have done anything fundamentally wrong? Please take a look at the attached files. TIA Portal V16 screenshots: [snip] Thanks! AttachmentScreenshots.zip (213 Downloads) |
Last edited by: Jen_Moderator at: 01/26/2021 10:10:48Removed links and added files as an attachment. |
|
Follow us on