6/10/2020 4:51 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71)
|
Hi RFIDNewb, first of all you need to download the GSD file from Balluf and import it into TIA Portal. Afterwards you can configure and set up your IO master. The file should be downloadable from here: I'm not familiar with those Balluff components. But I assume after configuring the IO master using the GSD file you should be able to load it into a PLC. Afterwards you might be able to watch some Bytes or Bits within the IO range of this master to understand what's going on when you put a RFID tag onto the reader. |
Follow us on