1/14/2007 12:00 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
[quote user="jaysandkays"]The control panel that I intend to interfacesome external inputsto is controlled by a Siemens 315-2DP CPU w/ a variety of existing Siemens analog input modules and Siemens digital input and digital output modules. The human interface is accomplished by way of a Siemens TP-27 touch panel. Can someone help get me started here with helping to: 1- locate necessary product programmingdocumentation for S7-300 series CPUs 2- identify necessary s/w for communicating w/ the 315-2DP to view/edit the code, as well as where I might be able to get it (the cheaper the better) 3- locate necessary product programming documentation for TP-27 HMI. 4- identify necessary s/w for communicating w/ the TP-27 to view/edit the code, as well as where I might be able to get it (the cheaper the better) Dear Jaysandkays, On your questions: 1. What do you want to program. I mean in which language STL, FUP, LAD...... 2. You may use STEP7 Lite : STEP 7 Lite V3.0 incl. SP2 Available for Downloadingit is for free, cheaper is not possible 3. TP27, TP37 Touch Panels 4. This TP might be programmed with Protool 6.0 SP3, you have to buy it. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to1 thankful Users |