7/17/2018 8:23 AM | |
Joined: 11/14/2013 Last visit: 10/13/2022 Posts: 3 Rating: (0) |
Hello guys, I have created program for testing device. At the end of test I create data log with active/non-active IO. That works fine. Now to my problem ... I need to download Data Log(.csv) from PLC automatically when the test is complete (or on demand on HMI) to server because of SAP. PLC - S7-1200 1214 DC/DC/DC 4.2 Is it possible ? Thank you for you response ------------------------------------------------------------------------------------------ |
Last edited by: Jiri Lan at: 7/17/2018 9:51:55 AMLast edited by: Jen_Moderator at: 7/17/2018 1:51:55 PMNew subject after splitting |
|
7/18/2018 6:18 PM | |
Joined: 7/7/2010 Last visit: 5/13/2024 Posts: 14710 Rating: (2359)
|
You can use the PLC's built in web server to download datalogs.
|
science guy |
|
7/18/2018 8:50 PM | |
Joined: 2/8/2017 Last visit: 3/15/2024 Posts: 87 Rating: (17) |
here is a imilar post and a solution how to perform an automatic download of a datalog via webserver:
|
This contribution was helpful to2 thankful Users |
Follow us on