4/7/2019 11:27 AM | |
Posts: 8 Rating: (0) |
I am also looking for this library as i need to migrate one project from PCS7 V7.1 to V9.0. As per this manual, this library supports upto PCS V8.1. So need this Library set up & replacement of the same library, which is compatible with PCS7 V9.0 S1 & Windows-10 64 Bit. If it is required to purchase, please provide the MLFB for the same, on priority basis.. Thanks..
------------------------------------------------------------------------------------------ |
Last edited by: Henish_STME at: 4/7/2019 11:28:55 AMLast edited by: Jen_Moderator at: 4/8/2019 12:00:34 PMNew subject after splitting |
|
4/7/2019 11:35 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
The old version of Modbus TCP no longer support by Siemens in a newer version of PCS. Even if you have the blocks and copy over to PCS 7 9.0, you will have to generate module error during chart compilation. See below link for new Modbus TCP for PN or CP. Modbus/TCP - Standardized and redundant Communication of PCS 7 with Third-Party Systems |
Last edited by: Jen_Moderator at: 4/8/2019 12:02:46 PMOptimized link. Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on