6/16/2021 12:45 PM | |
Joined: 12/27/2020 Last visit: 8/18/2022 Posts: 31 Rating: (0) |
Hello, I have Kind of similar Question. In my project, there are 7 stations in mfg. line and each station has 3-4 robots, convayor and doors which are controlled by PLC. Each station has one plc and the programmer has gave me 7 project/programme files for each station and by using block or functions from those files, i need to show all the actuators on a big scree (may be on TV) so that every person can watch mfg. line with it. if some fault happens then it should be in Red color, running process on Green/yellow color as shown in the attached png. file. I Need to create one more HMI for this Purpose? If yes then how can i use data in my new HMI Project from those 7 plc progeamme file? attached photo is example for 2 Station and i Need to prepare Display for 7 satations. Please do suggest. Thanks in Advance) ------------------------------------------------------------------------------------------ |
Last edited by: dbpathak at: 06/16/2021 12:49:04Last edited by: CS Moderator at: 06/16/2021 15:59:16New subject after splitting |
|
6/16/2021 4:02 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
closed cause question posted twice. The second thread with the subject GBA (Großbildanzeig/Large display screen) project is published within the same conference Visualization general Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on