1/9/2019 8:55 AM | |
Posts: 33 Rating: (0) |
Hi, I try to write the Example Image provided in the link to my SD card and it worked at first. Then when i try to turn on the IoT 2040, i saw the SD-LED didn't blink, so i read somewhere else that I need to re-write the SD card. And then, there is this Error 5: Access denied. I try all the methods such as go to properties=>security=>owner=> but there is no edit based on other website. It's just written "everyone". Another way i did was using command prompt=>run as administrator and it didn't work. Please help. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/11/2019 6:52:36 AMNew subject after splitting |
|
1/9/2019 9:40 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, did you try to ping the IOT2000 after turning it on? Or did you just assume that it isn't working? When do you get this error 5: access denied? Writing the image again or when you try to get connect to the IOT2000? Did you follow this document? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
1/16/2019 5:36 AM | |
Posts: 33 Rating: (0) |
I've tried to see the overview from command prompt and this is what happened. Any help will be appreciated. Thank you. |
1/16/2019 10:13 AM | |
Posts: 33 Rating: (0) |
Hi, I'm not sure if this is Engineering sample or MindConnect IoT. Below is the attachment |
1/16/2019 10:28 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, this is a SIMATIC IOT2040 - the correct device. If you have flashed the image (Example_Image_V2.2.0 downloaded from here) correctly according to the setting up and your LAN settings are correct, I can't imagine that.. Please check if the µSD card is plugged in correctly like this: Have you already tried to flash the image again or to use another µSD card? Which tool are you using to flash the Example Image to the µSD card? Best regards! |
Last edited by: bergmanu at: 1/16/2019 10:29:29 AMtypo Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on