6/18/2009 3:27 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi If you get the message, your PLC is usedover 75% with the OB-Cycletime. If you increase the limit, you get the message later, but nothing else change. Look if some function can run in a slower OB. You can look if you can use a second CPU for some function. You can look if you can use distribute controls. You should reduce the cycletime of your OBs. This helps you to calculate the cycletime: http://support.automation.siemens.com/WW/view/en/19688569 regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
11/9/2011 11:09 AM | |
Posts: 7 Rating: (0) |
is this error because ofDP slaves ....??? |
Follow us on