8/1/2017 9:11 AM | |
Posts: 648 Rating: (95) |
Deinstall V13 SP2 and install V14 SP1. Installation notes for V14 SP1: https://support.industry.siemens.com/cs/ww/en/view/109745460 WinCC V13 SP2 is not released for .NET Framework V4.7. V13 SP2 needs .NET Framework V4.5 WinCC V14 SP1 needs .NET Framework V4.6.2 Updates would normally released in two month rhythm. With best regards rh1990 |
Last edited by: rh1990 at: 8/1/2017 9:12:03 AM |
|
8/1/2017 4:13 PM | |
Joined: 11/15/2012 Last visit: 4/1/2024 Posts: 143 Rating: (8) |
Thanks for your information. Actually, V13 sp2 and V14 sp1 are separated product, it could be installed in one computer, we had tested in a PC and a virtual machine. For the old projects maintenance and license reason, we will be using both version for a time. |
8/2/2017 4:24 AM | |
Joined: 11/15/2012 Last visit: 4/1/2024 Posts: 143 Rating: (8) |
I have made reg file to to temporarily block installation of the .NET Framework 4.7 and reverse it. put four lines in block .net4.7.reg: Windows Registry Editor Version 5.00 unblock .net4.7.reg: Windows Registry Editor Version 5.00 Microsoft links: https://support.microsoft.com/en-us/help/4024204/how-to-temporarily-block-installation-of-the-net-framework-4-7 or you could use my uploaded files they are the same. DO NOT FORGET install 4.7 when Siemens releases an update to make compatible with .net 4.7. Attachmentblock and unblock .net 4.7.zip (217 Downloads) |
Last edited by: C.Change at: 8/2/2017 4:26:51 AM |
|
9/30/2017 3:03 AM | |
Joined: 11/15/2012 Last visit: 4/1/2024 Posts: 143 Rating: (8) |
update 3 for TIA Portal V14 sp1 is out, but there is still no info about compatibility about .NET 4.7 https://support.industry.siemens.com/cs/de/en/view/109747387 We have to wait. |
Follow us on