11/25/2019 8:32 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Hi Praytag,
Did you installed the software for Netlink? Starter needs an entry in the PG/CP interface settings, ibaPDA doesn't. |
iba AG - Data Acquisition and Analysis the way it should be |
|
11/25/2019 1:08 PM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
Sorry for asking this, but did you configure the NetLink to access the Profibus address of the drive, too? |
iba AG - Data Acquisition and Analysis the way it should be |
|
11/26/2019 10:26 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
I can't remember exactly, but you have to install the IBH config tool. There it is possible to config the address. |
iba AG - Data Acquisition and Analysis the way it should be |
|
12/2/2019 7:41 AM | |
Joined: 10/18/2006 Last visit: 7/9/2024 Posts: 120 Rating: (15) |
I am not sure if you can operate both software in parallel at the same time. As I understood both are working well, when not used together with the second? |
iba AG - Data Acquisition and Analysis the way it should be |
|
12/6/2019 5:24 AM | |
Joined: 4/19/2013 Last visit: 9/18/2024 Posts: 61 Rating: (0) |
Starter and SIMOTION don't go well with one another as we need anyone of them but, i am not sure about SimoCom |
Follow us on